KM_Space_Emergency_Inserted

KM Space_Emergency_Inserted

Address: 22944 (59A0H)
Type: WORD
Access: Read Only
Unit: --
Range: --
Default Value: --
Store Supported: No
Description:

This object contains the state of the internal emergency of Kollmorgen Space firmware.

Bit #

Name

Description

Default value

0

Protection_Drive_Current

1 = Drive is in current protection condition

0 = Ok

0

1

Protection_Open_Phase

1 = Drive is in open phase protection condition

0 = Ok

0

2

Protection_Drive_Voltage

1 = Drive is in voltage protection condition

0 = Ok

0

3

Protection_Drive_Thermal

1 = Drive is in thermal protection condition

0 = Ok

0

4

KM Space_User_Program

1 = Kollmorgen Space User Program Error

0 = Ok

0

5

Missing_Torque_Enable

1 = Torque Enable Input Missing (only for drive with Torque Enable Input)

0 = Ok

0

6

Watchdog_Occurred

1 = Watchdog Occurred

0 = Ok

0

7

EEprom_Fail

1 = EEprom Fail

0 = Ok

0

8

Internal_SW_Error

1 = Drive is in internal software  error condition.

0 = Ok

0

9

Feature_Unavailable

1= Kollmorgen Space Feature Unavailable

0 = Ok

0

10

Feedback_Error

1 = Motor Feedback Error

0 = Ok

0

11

Missing Calibration

1 = Missing Calibration

0 = Ok

0

12

Protection_EEprom_Write_Overrun

1 = EEprom Write Overrun.

0 = Ok.

0

13

KM Space_Software_Protection

1 = Kollmorgen Space software protection

0 = Ok

0

14

Protection_Current_Regulation

1 = Drive is in current regulation out of range protection condition

      Verify Motor Currents settings

0 = Ok

0

15

Protection_Open_Transistor

1 = Drive is in open transistor condition.

0 = Ok

0

Notes: --